shot3
Hey guys – I just released my second video for the rainbowduino ca...
ECG2_AM1
The ECG2_AM1 is a fully functional implementation of a 2-lead electrocar...
RGB LED Coffetable – Rainbow Carnival 2010 Entry
My entry for the Rainbowduino Carnival 2010 by seeedstudio A standalone ...
SLCD
Serial LCD It is a parallel to serial interface driver for 1602/0802LCD,...
Prototyping cables for *dunios
I wish some cables for my work – similar to this product: http://w...
Hb100; microwave; doppler; motion sensor; radar; proximity; speed;
I wish seeedstudio Could make a sensor boad with hb100 proximity dopler ...
adxl345 breakoutboard
Provide a adxl345 breakboard avaiable to use in a i2c ou sip, like board...
Compact power meter
It could be useful a compact power meter based on ACS756SCA-100B-PFF-T (...
Barometric Pressure Sensor
A Grove Twig with a barometric pressure sensor. This has many uses: alti...
Jaluino Bee board
Jaluino Bee is an open hardware, PIC based board, for DIYer. Bee is base...
soil moisture sensor for seeduino stalker
Hello, I’d like to have a soil moisture sensor able to work togeth...
TRF7970A_BreakoutBoard_Final
Hi, I have just designed an NFC BreakOut board based on the excellent  ...